Technical FAQs

Ask a Question

Does Vijeo Citect support LAN connection based of IPV6 address range.

As far as IPV6 support is concern presently citect only support IPV4 it do not support LAN connection based on IPV6 address range.
Was this helpful?
What can we do to improve the information ?