Technical FAQs

Ask a Question

How can I achieve RAID Hard Disk Redundancy in Magelis iPC range.

To achieve RAID Redundancy you need to install RAID system having one PCI and two redundant RAID Hard disk with 500 GB. The part reference number is HMIYRAIDPCI11. 

This is compatible with BOX PC, Panel PC 15" and Panel PC19" having atleast one PCI slot. 

Please find the attached document for configure RAID Redundancy in Magelis iPC.
 
Was this helpful?
What can we do to improve the information ?