Technical FAQs

Ask a Question

My Vijeo Citect alarms appears to be triggered correctly but the display time in alarm shows the current time not that time when the alarm is turned ON. How could this problem will be resolved.

This issue is caused if you have defined the {DATE,10} in your Summary Format Field in the Alarm Categories. Please note {DATE,..} is not a valid format field for Summary format, its valid only for Alarm Format. The field should be {ONDATE,..} and {OFFDATE,..} for the Summary format.  Kindly do these modification in Alarm Category & in INI file as shown in the attached snapshots for your reference. 
Was this helpful?
What can we do to improve the information ?