Technical FAQs

Ask a Question

When I write a command in button or rectangle properties under input section in Vijeo Citect, then there is restriction for number of characters in the field. Is there any alternate ways to program the same.

The Key Sequence Command in Vijeo Citect can be a maximum of 253 characters long. You can any command directly if it is withing 253 characters.

If the command is longer that that you should create a cicode function in the project and pass ArgValue1 as an argument for that cicode function. If you use cicode function this limitation will no longer exist.

For your better understanding please see the attached sample application. You can see the cicode function in file or you can directly launch cicode files from Vijeo Citect explorer.
Was this helpful?
What can we do to improve the information ?