Technical FAQs

Ask a Question

Is there any way to updated my Vijeo Citect Project from my IO Server machine to client machines.

To update the project changes from a server to all other servers & clients you can use the INI parameter [CtEdit]Copy parameter . On all the Vijeo Citect systems where you want to update the offline changes you need to configure this Copy parameter and give the Server`s User folder address which you can map on all the other Vijeo Citect client system. 
Was this helpful?
What can we do to improve the information ?