Technical FAQs

Ask a Question

Is it possible to use VW3A3409 encoder card in Altivar 71 drive.

VW3A3409 is the universal encoder card with SinCos, SinCos Hiperface®, EnDat® or SSI output.
So,VW3A3409 encoder card supports SinCos encoder technology.
Standard ATV71 drives are not compatible with VW3A3409 encoder card.
VW3A3409 encoder card is dedicated for the ATV71 S383 or ATV71Lift drives.
Was this helpful?
What can we do to improve the information ?