Technical FAQs

Ask a Question

Is it suitable to select Altivar 61 drive for Submersible motor application.

ATV61 is suitable for Submersible motor application.
However, following are the general recommendation for this application.
1. Insulation level of motor should be F class.
2. Do not use shielded cable.
3. Select Motor Choke/Sinus Filter depending on the Submersible motor cable length.
Was this helpful?
What can we do to improve the information ?