Technical FAQs

Ask a Question

Altivar 61 under monitoring, there is a motor power but the data is in terms of percentage. What does this percentage means.

[Motor power] (OPr) displays as a % of the rated motor power in the Monitoring Menu.
Example: 10 KW motor is connected to 10KW ATV61 drive.
Then 0% is 0 KW and 100% is 10KW.
Was this helpful?
What can we do to improve the information ?