Technical FAQs

Ask a Question

Why the input current of the ATV61HC50N4 drive is lower than the output current.

ATV61HC50N4 drive comes as standard with DC Choke.
The DC Choke decreases the amplitude of harmonics.
Then, the RMS current decrease. 
That is why; the input current of the ATV61HC50N4 drive is lower than the output current.
Was this helpful?
What can we do to improve the information ?