Technical FAQs

Ask a Question

What is the supply voltage range for ATS 48***Q & ATS 48***Y Soft starter.

Three-phase supply voltage range for ATS 48***Q is 230 - 15 % to 415 + 10 %.
Three-phase supply voltage range for ATS 48***Y is 208 - 15 % to 690 + 10 %.
Was this helpful?
What can we do to improve the information ?