Technical FAQs

Ask a Question

Is 490NOR00003 or 490NOR00005 HSBY fiber optic cable is Flame retardant.

yes , HSBY fiber optic cable i.e. 490NOR00003 or 490NOR00005  is Low Smoke Zero Halogen according to HD.624-7 and Flame-retardant according to NFC32 070 N°1 (C2) and CEI 332/1 .
Was this helpful?
What can we do to improve the information ?