Technical FAQs

Ask a Question

What could be the maximum length of a variable in Unity Pro v8.1

The maximum length of variable in Unity pro v8.1 is limited to 32 characters. If you make any variables which has more than 32 charecters Unity pro will give error while building the project.
Was this helpful?
What can we do to improve the information ?