Technical FAQs

Ask a Question

How can I access description of an AS-I slave connected to TSX ASY 1000 AS-i

Below is  the procedure for displaying the characteristics of a slave device:-

- In Unity Pro Open the AS-i module to be configured.
- Access the configuration screen by clicking on the tab Configuration. 
- Double click on the required slave.  Result: The window Associate a profile displays and highlights the device in question 
- Click on the button:
    View to access definition information,
    Details to access all the information.

Was this helpful?
What can we do to improve the information ?