Technical FAQs

Ask a Question

Can I access devices (via ping, PC tools) in a Quantum EIO network via the SERVICE port (ETH1) when it is configured in port mirror mode

No. When the SERVICE port is configured in port mirror mode, you cannot access devices — that is, you cannot ping other devices by connecting a PC to ETH1 in port mirror mode. When the SERVICE port is configured in access mode, then you can access devices in a Quantum EIO network via any tool.
Was this helpful?
What can we do to improve the information ?