Technical FAQs

Ask a Question

Why is the Ethernet link not working when I connect a PC to the SERVICE port

Do not connect a device with a speed in excess of 100 Mbps to the SERVICE port. If the device is configured for a speed that exceeds 100 Mbps, the Ethernet link may not be established between the device and the module through the SERVICE port.
Was this helpful?
What can we do to improve the information ?