Technical FAQs

Ask a Question

Is it possible to upload/download source code to M218 PLC if programmed with SoMachine V4.1

Source Upload / download is not supported on M218 PLC. It is a feature of PLC controller not software. So, irrespective of SoMachine version, it is not possible to upload / download the source code to M218
Was this helpful?
What can we do to improve the information ?