Technical FAQs

Ask a Question

What is the difference between “PARfactoryreset” and “PARuserreset” in Lexium 32 drives

PARfactoryset = YES set all the parameters to default values and these saved to EEPROM.

PARuserrest = YES or bit 0 from Modbus or Fieldbus set all parameters to default values except
  • Communication parameters
  • Inversion of direction of movement
  • Selection of signal type for PTI interface
  • Setting of encoder emulation
  • Function of digital inputs / outputs
and these settings are not saved to EEPROM
Was this helpful?
What can we do to improve the information ?