Technical FAQs

Ask a Question

Why ATV-process drives ( ATV6xx) can not be seen with SoMove Lite software

The major innovation of SoMove V2.0 consists in the dissociation of the executable common part (FDT) on all devices and a product specific data base for each product (DTM).
So, it requires (1) Installation of SoMove V2.0 FDT and then (2) Install DTM libraries according to device range you need to configure.
There is a DTM available for ATV process  (ATV6xx) drive and user need to install it post successful installation of SoMove FDT .
Please, refer to the below link to download ATV process (ATV6xx)
http://www.schneider-electric.com/download/WW/EN/results/0/4889330-DTM-files/336700273-Altivar-Process/0/?showAsIframe=true
 
Was this helpful?
What can we do to improve the information ?