Technical FAQs

Ask a Question

What is the maximum numbers of connections supported by Embedded Ethernet port of Altivar process (ATv6xx) drive

Maximum 32 numbers of concurrent connections (TCP/IP  and / or UDP/IP) are supported by embedded Ethernet port
Was this helpful?
What can we do to improve the information ?