Technical FAQs

Ask a Question

How “Stop and Go” function could be activated

“Stop and Go” could be activated with any of option below
 
  1. Could be activated automatically if drive is in STOP mode and post Programmable time – idLN [Energy saving delay] period lapses
  2. Activation via Network communication
  3. Activation via Logic Input
Was this helpful?
What can we do to improve the information ?