Technical FAQs

Ask a Question

What are the advantages of the ZBPA, ZBP0 and ZBP0A clear pushbutton covers for the Harmony XB4 and XB5 range pushbutton switches?

The use of a clear pushbutton cover offers IP69K degree of protection, which provides resistance to:
  • Water ingress from high pressure washers (Karcher)
  • Salt spray 

Here is the list of cover part numbers:
  • ZBPA:    covers for flush pushbuttons with circular head
  • ZBP0:    covers for projecting pushbuttons with circular head
  • ZBP0A: covers for flush or projecting pushbuttons with circular head for food & beverage applications
A cover cannot be used with a legend holder.
Clear, round, self-adhesive legends are required (type ZBY1101).
Resistance to salt spray
Was this helpful?
What can we do to improve the information ?