Technical FAQs

Ask a Question

Using the Wi-Fi access point and antenna module PMXNOW0300 what is the maximum distance between transmitter & receiver is recommended for communication.

The maximum distance between Wifi transmitter and receiver is limited to 300 mtrs line of site and this can be extended upto 5 Km with the use of external antenna. 
 
Was this helpful?
What can we do to improve the information ?