Technical FAQs

Ask a Question

For the XB4BS84441, BS8444 & BS8445 what will be the travel distance when the head is entirely pushed.

The maximum travel distance between the released state and the actuating state is 4mm in Harmony XB4BS84442, BS8444 & BS8445.
Was this helpful?
What can we do to improve the information ?