Technical FAQs

Ask a Question

I am getting message "Class not registered " when use the ActiveX DatabaseExchange.DataManager in Vijeo Citect V7.30.

There may be some corruption in the registry settings in the database exchage active x file due to which you were getting that message whe using DataBase Exchange in Vijeo Citect`s graphics page. We recommend to re-register this DatabaseExchange.DataManager.ocx file as per the attached below procedure.
Was this helpful?
What can we do to improve the information ?