Technical FAQs

Ask a Question

Can we send Email from Vijeo Citect without using any of the Email Client software such as Outlook.

Vijeo Citect MAPI (Messaging Application Program Interface) functions also known as Mail Functions, are designed to work with the Microsoft standard Messaging API set. This means that if you have a Microsoft compliant E-Mail system you should be able to access standard internet E-mail using programs such as Outlook, Inbox, Exchange Server etc. This then allows the Citect Mapi functions to send mail out using SMTP mail services. 

Thus to send SMS using Vijeo Citect SCADA you should have one Email Client application program which support Microsoft standard Messaging API set. 
Was this helpful?
What can we do to improve the information ?