Technical FAQs

Ask a Question

How to open and Numeric Keypad when I click on any Numeric Display in Vijeo Citect Runtime to update a new numeric value.

To open a keypad when you click on a numeric display in Vijeo Citect Runtime, you will have to use the Function Called FormNumPad in your project.
To use this function open the property of Numeric Display and in Input Tab under Up Command write down the following syntax:

<variable name to write>= FormNumPad("<title of the num pad>", <variable name to write>, <mode of the keypad>);

Now when you click on the variable in Runtime you will see a popup keypad according to the Mode you have selected on screen to put a new value.

For more detail on the function, see attached document.
Was this helpful?
What can we do to improve the information ?