Technical FAQs

Ask a Question

What will be the Maximum operational Power rating for the LC1F1250 & LC1F1400 contactor in AC-1 category.

The Maximum operational Power rating for LC1F1250 and LC1F1400 contactor in AC-1 category as given below in attachment.
Was this helpful?
What can we do to improve the information ?