Technical FAQs

Ask a Question

What is the nominal volatge tolerance of Acti9 RCDs.

The Acti9 RCD devices are compliant with the standards IEC/EN 61008 & 61009 that defines tolerance of -10% - +5% of nominal voltage.
Was this helpful?
What can we do to improve the information ?