Technical FAQs

Ask a Question

Is it possible to use Multi9 C60 (UL1077 or UL489) for an operating voltage of 24V DC.

The Multi9 C60 circuit breakers (UL1077 or UL489) can be used for an operating voltage of 24V DC. 
Was this helpful?
What can we do to improve the information ?