Technical FAQs

Ask a Question

What is the function of 24 V DC power-supply terminal block LV434210 of Compact NSX range.

The 24 V DC power-supply terminal block is required to power the trip unit when the trip unit is not connected to a FDM121 display unit and the communication system. When used, it excludes the connection of NSX cord and it can be installed only with NSX Micrologic 5/6 trip units.
Was this helpful?
What can we do to improve the information ?