Technical FAQs

Ask a Question

What will be the part references for the Pilot Lights with supply voltage 400 Vac, LED lamp, dia 22 mm with red, yellow, blue and green colours.

You  can use our Harmony XB4 range XB4 BV5** (Pilot lights with integral LED and transformer (1.2 VA, 24 V secondary) for 22 mm dia .
Below are the part reference as follows :
  • Green Colour : XB4 BV5B3 
  • Red Colour : XB4 BV5B4 
  • Orange Colour : XB4 BV5B5 
  • Blue Colour : XB4 BV5B6 
Was this helpful?
What can we do to improve the information ?