Technical FAQs

Ask a Question

Which driver I can use in Vijeo Citect for IEC 104 communication. Do we need to purchase any separate license for that driver.

In Vijeo Citect latest versions we have only communication driver available for IEC 60870-5-104 which is also a speciality driver and needs to be purchased separately.
Was this helpful?
What can we do to improve the information ?