Technical FAQs

Ask a Question

Can we use TM2AMM6HT as a direct replacement for TWDAMM6HT and will this replacement require for change in programming also .

TM2 range has totally substitute the TWD range and it became the unique I/O expansion module range, compatible both with Twido bases, M238 bases and Advantys OTB Distributed I/O bases. 
 
You can use TM2AMM6HT as a direct replacement for TWDAMM6HT without any programming changes, only you need to select TM2 in TwidoSuite software and it will work. There is not any compatibility issue using this replacement. 
Was this helpful?
What can we do to improve the information ?