Technical FAQs

Ask a Question

Which pressure sensor we can select for use in Nitrogen gas environment.

You can use our XMLA series to detect the nitrogen gas . The nitrogen is a neutral gaz,and you can control it without problem with the pressure switch XML. For nitrogen, choose an XML product with corrosive fluids version, because the standard diaphragm doesn`t resist against nitrogen gas. The best product to measure a pressure of 2.5 bar is XMLA004C2S11.
Was this helpful?
What can we do to improve the information ?