Technical FAQs

Ask a Question

Is Altivar 312 drives confirms the IEC 60721-3-3 standard.

On ATV312 drives, a coated card comes as standard (IEC 60721-3-3 Classes 3C2).
Was this helpful?
What can we do to improve the information ?