Technical FAQs

Ask a Question

What is the programming parameter of Motor pole on Altivar 212 drive.

The programming parameter of Motor Pole on ATV212 is F856.
 
Example:
 
Program F856 => 2 [4 poles] 

So, 2 means, motor have 4 poles. It means Motor will run at 1500 rpm.
 
Was this helpful?
What can we do to improve the information ?