Technical FAQs

Ask a Question

Is it possible to use class E insulation Motor with Altivar 71 drive.

It is advised to have class F insulation Motor for the windings to use with ATV drives. 

It is not recommended to use class E insulation motor with ATV because motor will heat & insulation will weak and after that motor may burn.
Was this helpful?
What can we do to improve the information ?