Technical FAQs

Ask a Question

What is the material of ZCKE08 limit switch head (both spring rod & body).

Material of spring rod is X12 CrNi 18-10 (DIN designation) which is a stainless steel spring. 

ZCKE08 body uses mainly zamak or zinc alloy material. 
Was this helpful?
What can we do to improve the information ?