Technical FAQs

Ask a Question

Is it possible to save Homing Method to Stepper drives SD328 range. If yes, how to save.

For Stepper driver range SD328, firmware version V1.501 or higher include parameter “SaveHomeMethod” that allows to save preferred homing method. The meaning of the values of the parameter SaveHomeMethod corresponds to the meaning of the values of the parameter
HMmethod.
When the device is switched on, the value in the parameter HMmethod is overwritten by the value set in the parameter SaveHomeMethod. 
 
Was this helpful?
What can we do to improve the information ?