Technical FAQs

Ask a Question

Is it possible to use Altivar 71 drive with synchronous motor and encoder feedback signal of type SinCos 1 Vpp.

Yes, it is possible to provide speed feddback of signal SinCos 1 Vpp to ATV71 drive.
For this user must use ATV71H***N4383 drive(V1.7 and higher)  and encoder card should be univeral encoder card having part reference VW3A3409.
 
Was this helpful?
What can we do to improve the information ?