Technical FAQs

Ask a Question

How to set SNMP parameters on an EGX100 or EGX300 to view the networking status and diagnostics the gateway

EGX100 and EGX300 support SNMP protocol only on allowing a network administrator to remotely access an EGX with an SNMP manager (SNMP Server), and view the networking status and diagnostics in the MIB2 format.

There is no need to download any MIB file to the EGX because the MIB II standard only provides basic informations.

Attached are some screen captures to show a possible setting of the SNMP parameters.

It is not possible to view data from downstream meters via SNMP.
Was this helpful?
What can we do to improve the information ?