Technical FAQs

Ask a Question

Why PM810 Min/Max value reset on auxiliary control power recycle.

There could be the reason that the PM810 without log module, does not have a BIOS battery.  
Because, PM810 is without datalog module if control power is lost, no min/max values can be saved.
Was this helpful?
What can we do to improve the information ?