Technical FAQs

Ask a Question

Difference between BE700Y-IN and BE700Y-IND

The difference between BE700Y-IN and BE700Y-IND is only the change in the battery capacity of the UPS (Uninterrupted Power Supply), rest all technical specifications remains same.

The battery capacity of models is mentioned below in the table.
UPS Model Number Battery Capacity
BE700Y-IN 12AH, 12V (1 battery)
BE700Y-IND 9AH, 12V (1 battery)
Was this helpful?
What can we do to improve the information ?