Technical FAQs

Ask a Question

Is it possible to connect Altivar 61/71 drive to a power feeder whose short-circuit capacity exceeds the drive short-circuit current rating listed on the catalogue.

It is forbidden to connect the drive to a power feeder whose short-circuit capacity exceeds the drive short-circuit current rating listed on catalogue.

Example: Maximum prospective line Isc of main supply is 22 kA for ATV61HD55N4 & ATV61HD75N4. 
So, it is not allowed to connect ATV61HD55N4 & ATV61HD75N4 drives to a power feeder whose short-circuit capacity exceeds 22kA.
Was this helpful?
What can we do to improve the information ?