Technical FAQs

Ask a Question

How we can name and address each channel of IO module on RIO of M580.

User can use this address as channel value of modules available on RIO, this comes from Device DDT and also it is unlocated so user can not put a located address for this variables. So to assign a name and address user need to map this address. Refer the attached video file to understand how to map Device DDT variable to physical memory.

Download the attached video from below mentioned link:

Was this helpful?
What can we do to improve the information ?