Technical FAQs

Ask a Question

Getting message "Config.nt.The system is not suitable for running MS-Dos and Microsoft windows applications" while trying to run Concept v2.6 SR7.

This message is moreover related to Windows setting not with Concept Software.

To work around this issue, follow these steps:
  1. Click Start, point to Settings, and then click Control Panel.
  2. Double-click System, click the Advanced tab, and then click Environment Variables.
  3. In the User variables for User_Name list, click TMP, and then click Edit.
  4. In the Variable value box, type c:\winnt\temp, and then click OK three times.

    Alternatively, type the path of any folder that does not use long file names in the Variable Value box.
  5. Close Control Panel.
Was this helpful?
What can we do to improve the information ?