Technical FAQs

Ask a Question

what is the Attenuation limit of Coaxial cable RG6 and RG11.

Below is the Attenuation limit of RG6 and RG11 at 1.544MHZ:

97-5750-000 RG6 cable has 1.18dB/100m (0.36dB/100ft) attenuation at 1.544MHz.
97-5951-000 RG11 cable has 0.56dB/100m (0.17dB/100ft) attenuation at 1.544MHz.
Was this helpful?
What can we do to improve the information ?