Technical FAQs

Ask a Question

Are Compact INS/INV switch disconnectors suitable for Installation in class II switchboards.

All Compact INS/INV switch-disconnectors are class II front-face devices. They may be installed through the door of class II switchboards (as per standard IEC 60664) without downgrading switchboard insulation. Installation requires no special operations even when the switch-disconnector is equipped with rotary handles.
Was this helpful?
What can we do to improve the information ?