Technical FAQs

Ask a Question

Do the Compact INS/INV switch-disconnectors meet the environmental requirements (tropicalisation) of the IEC standards.

The Compact INS/INV switch-disconnectors meet the environmental requirements of the following standards:
> IEC 60068-2-1 - dry cold (-55 °C)
> IEC 60068-2-1 - dry heat (+85 °C)
> IEC 60068-2-30 - damp heat (95 % relative humidity at +55 °C)
> IEC 68-2-52 (level 2) - salt mist.
Was this helpful?
What can we do to improve the information ?