Technical FAQs

Ask a Question

What is the Degree of protection of Compact INS/INV switch-disconnectors.

The Compact INS/INV switch-disconnectors offer the following protection characteristics depending on the installation conditions:
> IP: degree of protection (standard IEC 60529)
> IK: protection against external mechanical impacts (standard EN 50102).
Was this helpful?
What can we do to improve the information ?